You can depend on Cummins to deliver the leading technology for 2010 and beyond. Cummins is the only engine manufacturer with a single, integrated system that encompasses critical subsystems from air intake to exhaust after treatment.
Cummins 2010 on-highway engines use proven technology and the same core components that make today's Cummins engines so fuel-efficient and reliable. Cummins Heavy-Duty ISX15 and ISX12 and MidRange engines will use the Cummins Aftertreatment System, including Selective Catalytic Reduction (SCR) that is already working in hundreds of thousands of commercial vehicles across Europe. The Cummins truck engine line-up includes the following diesel engines:
Cummins reliability and performance is also available in a natural gas option. For information on Cummins natural gas engines for truck and bus applications, visit Cummins Westport.
For more information on Cummins Truck Engines, contact the nearest Cummins Power Systems branch to speak with a truck engine specialist or visit the Cummins On-Highway Engines website.
© 2011 - – Cummins Power Systems, LLC. All Rights Reserved. Site by Shanahan Design